DOCA0197EN-01

Firmware Update

Presentation

Use the latest version of EcoStruxure Power Commission App for all firmware updates.

All firmware designed for the Wireless Panel Server is signed using the Schneider Electric public key infrastructure (PKI).

Checking the Firmware Version

The current Wireless Panel Server firmware version can be checked with EcoStruxure Power Commission App.

Updating Firmware With EcoStruxure Power Commission App

If the Wireless Panel Server is not updated to the latest firmware version, firmware update can be done using EcoStruxure Power Commission App.

The prerequisites for updating the firmware with EcoStruxure Power Commission App are the following:

  • The latest version of EcoStruxure Power Commission App must be downloaded and installed on the smartphone.

  • The smartphone must be connected to the Wireless Panel Server through Bluetooth connection.

At the end of the firmware update process, the Wireless Panel Server needs to reboot (see Rebooting Wireless Panel Server ).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.