Configure Fiber Manager Reports

Fiber Manager provides several different asset reports.

IMPORTANT: For all reports except the Cable Report, Fiber Manager supports Internet Explorer or Edge in Internet Explorer Compatibility Mode. To turn on the Compatibility Mode in Edge, follow these steps:
  1. In Edge, click the Settings and More ellipsis in the upper, right-hand corner.

  2. Click Settings.

  3. Click Default Browser.

  4. Under Internet Explorer Compatibility, leave the “Let Internet Explorer open sites in Microsoft Edge” at the default setting of “Incompatible sites only (Recommended).”

  5. For “Allow sites to be reloaded in Internet Explorer mode,” choose “Allow.”

  6. For “Internet Explorer mode pages,” click the Add button and add the following entries. Adding these entries avoids the extra step of having to “Reload in Internet Explorer mode.” Be sure to edit the username in the URL to an appropriate value:

    1. file:///C:/Users/username/Documents/ArcFM%20Solution/Fiber%20Manager/Reports/Allocation_Report.xml

    2. file:///C:/Users/username/Documents/ArcFM%20Solution/Fiber%20Manager/Reports/Glass_Report.xml

      IMPORTANT: The Patch Panel Connection, Splice, and Trace Reports are not added here because the URL contains information specific to the chosen splice and are therefore not generic URLs. These reports initially open on a blank tab. After this initial attempt to render the report, click the Settings and More ellipsis in the upper, right-hand corner, then choose “Reload in Internet Explorer mode.”

All reports come with an example .xsl stylesheet. By default, this stylesheet and all generated reports are found in the folder C:\Users\username\Documents\ArcFM Solution\Fiber Manager\Reports.

If needed, you can change the location of the stylesheets and destination for generated reports. Fiber Manager saves report files to a root folder based on the user's “My Documents” system setting. Specifically, Fiber Manager references the value for “Personal” saved in the registry key “Computer\HKEY_CURRENT_USER\Software\Microsoft\Windows\CurrentVersion\Explorer\User Shell Folders” when determining the default folder in which to write reports.

If it does not find this folder, it will attempt to create it and copy the default .xsl files as saved in the “ArcFM Solution\Fiber Manager\Reports” for All Users.

TIP: This is particularly helpful when you want to change the underlying .xsl stylesheet. After performing your updates, place the stylesheet in the “All Users” copy of the Fiber Manager reports directory. Instruct your users to delete the existing copy in their local directory. The next time a report is run, the application will grab the updated stylesheet.

Add Additional Fields to Reports

You can customize your reports in Fiber Manager by adding one or more additional fields to each report. For example, in addition to the fields that appear in the Fiber Trace Report by default, you might also want to display attribute values from the Fiber Availability, Fiber Status, and Comments fields. Or, in the Splice Report, you may want to see Device Name values and the Tray on which fibers are spliced.

Add the following field model names to any field on any feature or object class. Use the field model name that corresponds to each report.

Report Name

Field Model Name

Fiber Allocation Report

FIBERALLOCATIONREPORTFIELD

Fiber OTDR Trace Report

FIBEROTDRREPORTFIELD

Fiber Circuit Trace Report

FIBERCIRCUITREPORTFIELD

Patch Panel Connection Report

FIBERPPCONNFIELD

Splice Report

FIBERSPLICEREPORTFIELD

Fiber Trace Report

FIBERTRACEREPORTFIELD

You can add the same field model name to multiple fields. The values in the fields to which these model names are assigned will appear so long as the corresponding object belongs in the fiber object hierarchy. In other words, assigning these fields to an exclusively-electric feature class, for example, does not have any effect on these reports and the value is not displayed.

Primary Display Field

All reports utilize the ArcFM Primary Display field for reportable fiber object and classes. Ensure an appropriate and useful field is chosen for fiber features. You can change the ArcFM Primary Display field setting in the Field Display tab of the ArcFM Properties Manager.

Company Logo

All reports reference a placeholder “Logo.jpg” file, located in the “ArcFM Solution\Fiber Manager\Reports” directory. The easiest way to change the logo is to simply replace the placeholder logo with your own, but maintain the same file name. In this manner, you do not need to update the stylesheet. Alternatively, you can change the filename, but then you also need to change the filename among all stylesheets to match.

Patch Panel Connection Report

Ensure the PATCHLOCATIONREPORTABLE class model name is assigned to the feature class representing patch locations. This model name enables you to select the patch location feature class with the Patch Panel Connection Report tool.

Customizing the Stylesheet

Using a preferred editor application, you can customize the look and feel of the reports by updating the .xsl stylesheet. For more instructions and a downloadable example, read the myArcFM article Enhanced Fiber Splice Report.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.