Fiber Enclosure Model

TIP: This domain is not required but contains the model names/numbers that can be used in conjunction with Fiber Enclosure Manufacturer.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

3M - Fiber Dome (FD06)

3M - Fiber Dome (FD06)

3M - Fiber Dome (FD08)

3M - Fiber Dome (FD08)

3M - Splice Case (2178-LL)

3M - Splice Case (2178-LL)

3M - Splice Case (2178-LS)

3M - Splice Case (2178-LS)

Coyote 00415 without Drop

Coyote 00415 without Drop

Coyote 004151 with Drop

Coyote 004151 with Drop

Other

Other

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.