Fiber Units of Measure

TIP: This domain is not required but serves as a multiplier for distance calculations when cable length is updated via an AU.

Properties:

  • Field Type: Integer

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

3

Feet

5

Miles

9

Meters

10

Kilometers

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.