Fiber Availability Indicator

TIP: This domain is not required, but it populates a required field value and is used for indicating which fibers are available or unavailable.

Properties:

  • Field Type: Integer

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

0

Unavailable

1

Available

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.