Manually Create Schema and Configure

If you prefer, you can manually create the necessary domains, and feature and object classes in the sample Fiber schema. This requires that you create and assign the model names, assign the autoupdaters, and set default values and aliases.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.