Fiber Port Function

TIP: This domain is not required, but you can use it to track port function

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Primary Receive

Primary Receive

Primary Transmit

Primary Transmit

Secondary Receive

Secondary Receive

Secondary Transmit

Secondary Transmit

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.