Fiber Optic Cable Installed Tension

TIP: This domain is helpful for documenting installed tensions. It does not factor into any length calculations performed by the application.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

2254

2254

2884

2884

3251

3251

3358

3358

3399

3399

Other

Other

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.