Fiber Overhead Underground

TIP:
  • This domain is not required but it tells the glass report into which category to put a particular cable’s glass length. These values don’t have to be stored in a domain, but doing so means less typing for users.

  • Overhead and Underground coded values should always be included in this domain. Other values are optional.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Bridge

Bridge

Direct Buried

Direct Buried

Overhead

Overhead

Underground

Underground

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.