Convert to ArcFM Objects

The Fiber dataset and all Fiber tables, except the F_CIRCUITCOMPONENT table, must be converted to ArcFM objects.

  1. In ArcCatalog, navigate to the Fiber dataset, then click it once to highlight in blue.

  2. In the Contents pane, select the fiber feature classes.

  3. Right-click anywhere in the highlighted set and choose ArcFM Solution Object Converter.
  4. Select Convert to use ArcFM objects and click OK.

  5. Regarding the fiber object tables, in the Catalog Tree click the geodatabase once to highlight it in blue.

  6. In the Contents pane, select the fiber object tables.
    IMPORTANT: Do not convert the F_CIRCUITCOMPONENT table. Leave this as an Esri object for best performance.

  7. Right-click anywhere in the highlighted set and choose ArcFM Solution Object Converter.
  8. Select Convert to use ArcFM objects and click OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.