Define Points and Lines

TIP: If you're creating an object class (table), skip the steps in this topic. These settings apply only to features with spatial representation on the map.

If you haven't already, determine your feature's geometry (Table 3 on the worksheet): point or line. If you have a line feature, create it as an ArcFM Complex Edge feature. If you have a point feature, create it as an ArcFM Simple Junction feature. 

Point Feature Settings

Point features can have certain properties (e.g., splitting fiber lines) which use specific class model names, fields and autoupdaters. The following table describes the class model names, fields and autoupdaters used by point features.

TIP:

Using the Settings for Point Features Table

  • The Example Field Name and Data Type columns contain values entered while creating the feature. If using the worksheet, record these values in Table 5.

  • The Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.

  • The Class Model Name column contains values entered in the ArcFM Properties Manager on the Model Names tab. If using the worksheet, record these values in Table 4.

  • The Object Autoupdaters row contains the object autoupdaters entered in the ArcFM Properties Manager on the Object Info tab. If using the worksheet, record these values in Table 6.

Settings for Point Features Table

Function

Settings

 

Example Field Name

Data Type

Field Model Name

Class Model Name

Modifiable by Location Editor

     

LOCATIONEDITABLE

Represents length but does not split cables

 Length

Double

POINTLENGTH

 

Object Autoupdaters:

  • On Feature Create: ArcFM Fiber Optic Cable Length

  • On Feature Update: ArcFM Fiber Optic Cable Length

Splits cable lines

       

Object Autoupdaters:

  • On Feature Create: ArcFM Fiber Optic Cable Splitter

  • On Feature Update: ArcFM Fiber Optic Cable Splitter

Splits cable lines and has editable connections

     

 FIBERCONNECTIONCONTAINER

Object Autoupdaters:

  • On Feature Create: ArcFM Fiber Optic Cable Splitter

  • On Feature Update: ArcFM Fiber Optic Cable Splitter

Represents a change in a linear feature's field

     

TRANSITIONPOINT

(Transition points are ignored when running the Allocation Report)

Object Autoupdaters:

  • On Feature Create: ArcFM Fiber Optic Cable Splitter, ArcFM Validate Transition Point Creation

  • On Feature Update: ArcFM Fiber Optic Cable Length

Line Feature Settings

Linear features can have certain properties, such as appearing in the glass report, which use specific class model names, fields and autoupdaters. The following table describes the class model names, fields and autoupdaters needed for line features with the following functions.

TIP: Using the Settings for Line Features Table
  • The Example Field Name, Data Type, and Domain columns contain values entered when creating the feature. If using the worksheet, record these values in Table 5.

  • The Assign Field Model Name column contains values entered in the ArcFM Properties Manager on the Field Model Names tab. If using the worksheet, record these values in Table 5.

  • The Assign Class Model Name column contains values entered in the ArcFM Properties Manager on the Model Names tab. If using the worksheet, record these values in Table 4.

  • The Object Autoupdaters row contains the object autoupdaters entered in the ArcFM Properties Manager on the Object Info tab. If using the worksheet, record these values in Table 6.

Settings for Line Features Table

Function

Settings

 

Example Field Name

Data Type

Field Model Name

Class Model Name

Modifiable by Location Editor

     

LOCATIONEDITABLE

Contains connectable objects and tracks length

 EndFootStamp

Long Integer

ENDFOOTSTAMP

 

StartFootStamp

Long Integer

STARTFOOTSTAMP

 

FieldNotesLength

Double

FIELDNOTESLENGTH

 

SheathLengthSource

Text

SHEATHLENGTHSOURCE

(assign the "Fiber Optic Cable Length Source" domain to this field)

 

TwistFactor

Double

TWISTFACTOR

 

GlassLength

Double

GLASSLENGTH

 

SegmentGlassLength

Double

SEGMENTGLASSLENGTH

 

SheathLength

Double

SHEATHLENGTH

 

SegmentLength

Double

SEGMENTLENGTH

 

Object Autoupdaters:

  • On Feature Create: ArcFM Fiber Optic Cable Length

  • On Feature Update: ArcFM Fiber Optic Cable Length

  • After Feature Split: ArcFM Validate Fiber Sheath Split

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.