Fiber Glass Grade

TIP: This domain is not required but can track the grade of a particular fiber. For example, zero water peak fibers have lower loss than low water peak fibers across the entire spectrum.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Leaf

Leaf

Low Water Peak

Low Water Peak

Water Peak

Water Peak

Zero Water Peak

Zero Water Peak

Other

Other

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.