F_SplitterInputPort_SplitterOutputPort

You can find existing relationships and create new ones in ArcCatalog. Almost all relationships are found at the geodatabase level, as opposed to the dataset level. Below is an image of the final properties for this relationship. For more information about these settings, see the relationship topic Summary of Recommendations.

Because this is a “sibling” relationship, it does not require any autoupdaters set at the relationship itself:

  • On Relationship Created: <None>

  • On Relationship Deleted: <None>

IMPORTANT: This relationship is for the splitter being modeled as a related object table to a splitter feature class. In other words, it is for the splitter with the model name SPLITTER. This splitter is not supported by Wavepoint. The names of tables, relationships, and fields do not matter to Fiber Manager. Fiber Manager only cares about the model names assigned to the tables, relationships, and fields. Here, the model name is being used as the relationship name to differentiate the two splitter data architectures.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.