FiberOpticCable

IMPORTANT:
  • ObjectID fields are automatically created (by Esri) when you create the schema.

  • GlobalID fields are required by Fiber Manager and are created with Esri's Add Global ID tool (Manage > Add Global IDs).

  • GlobalID fields must also have the GLOBALID field model name assigned.

  • Enabled fields are automatically added/configured by the geometric network.

  • In ArcGIS applications, there are four numeric data types: Short Integer, Long Integer, Float, and Double. The choices reflect a balance between minimizing storage space while still allowing enough range and precision for the field to be useful. For example, because lengths typically have decimals, these fields are assigned either Float or Double.

    In the table below, any field set to integer does need to be either a Short or Long Integer, as these fields cannot contain decimals. So, the decision comes down to the minimum and maximum values you need for the field:

    • Short Integer Storable Range: -32,768 to 32,767

    • Long Integer Storable Range: -2,147,483,648 to 2,147,483,647

    So, as an example, would you ever have more than 32,767 patch panels on a single rack? No. So, the RackPosition field for Patch Panels could be a Short Integer. Conversely, foot or meter stamps along a cable could exceed 32,767. So, CableMarking fields for fiber optic cables should be a Long Integer. Our integer recommendations err on the side of more range and usefulness, but your company could decide to change a Long Integer to a Short Integer (or a Double down to a Float) if you knew the maximum values would never exceed the types’ upper threshold.

Alias: Fiber Optic Cable

Type of features: ArcFM Complex Edge Feature

Geometric Network: Ultimately belongs to the Fiber_Network when you Create the Geometric Network later in these steps.

TIP: You can change the length of Text fields to a number that is appropriate for your organization.

Field

Data Type

Default Value

Domain

Length/Precision

CableLength

Alias: Cable Length

Double

     

CableLengthSource

Alias: Cable Length Source

Text

 

Fiber Optic Cable Length Source

50

CableMarkingUnitOfMeasure

Alias: Unit of Measure

Long Integer

 

Fiber Units of Measure

 

CableName

Alias: Cable Name

Text

   

50

CableOwner

Alias: Owner

Text

 

Fiber Owner

50

CableTwistFactor

Alias: Twist Factor

Double

     

CableType

Alias: Type

Text

 

Fiber Optic Cable Type

50

EndingCableLengthMarking

Alias: Ending Cable Length Marking

Long Integer

     

EstSMAttenuation1310

Alias: Estimated SM Attenuation 1310

Double

     

EstSMAttenuation1550

Alias: Estimated SM Attenuation 1550

Double

     

FiberChildClassModelName

Alias: Fiber Child Class Model Name

Text

BufferTube

 

50

FiberCount

Alias: Strand Count

Long Integer

 

Fiber Number of Strands

 

FiberParent

Alias: Fiber Parent

Guid

     

FiberParentClassModelName

Fiber Parent Class Model Name

Text

   

50

FieldNotesLength

Alias: Notes Length

Double

     

GlassLength

Alias: Glass Length

Double

     

InstalledBy

Alias: Installed By

Text

 

Fiber Contractors

50

MultimodeAvailabilityQty

Alias: Multimode Availability Quantity

Long Integer

     

OverheadUnderground

Alias: Overhead Underground

Text

 

Fiber Overhead Underground

50

SegmentGlassLength

Alias: Segment Glass Length

Double

     

SegmentLength

Alias: Segment Length

Double

     

SinglemodeAvailabilityQty

Alias: Singlemode Availability Quantity

Long Integer

     

StartingCableLengthMarking

Alias: Starting Cable Length Marking

Long Integer

     

ThisFiberClassModelName

Alias: This Fiber Class Model Name

Text

Sheath

 

50

Field Display

Primary Display Field: Choose this field in the ArcFM Properties Manager. The chosen field is displayed when using ArcFM tools such as the ArcFM Locator and ArcFM Attribute Editor. Your company can choose the most useful field to display for the end users. If the chosen field is null for the selected or identified features, the display field defaults to the ObjectID.

Model Names

FIBERDATATABLESOURCE, FIBEROBJECT, LOCATIONEDITABLE, SHEATH

Field Model Names

CableLength: SHEATHLENGTH

CableLengthSource: SHEATHLENGTHSOURCE

CableMarkingUnitsOfMeasure: MARKINGUNITSOFMEASURE

CableName: FIBERCIRCUITREPORTFIELD, FIBERCONNECTIONDISPLAYFIELD, FIBEROTDRREPORTFIELD, FIBERTRACEREPORTFIELD, SHEATHID, SCHEMATICEXPORTATTRIBUTE

CableOwner: FIBERTWOPOINTTRACEFIELD

CableTwistFactor: TWISTFACTOR

CableType: SHEATHTYPE, FIBERTWOPOINTTRACEFIELD

EndingCableLengthMarking: ENDFOOTSTAMP

EstSMAttenuation1310: ATTENUATIONAFREQ

EstSMAttenuation1550: ATTENUATIONBFREQ

FiberChildClassModelName: FIBERCHILDCLASSMODELNAME

FiberCount: NUMBEROFSTRANDS, FIBERTWOPOINTTRACEFIELD

FiberParent: FIBERPARENT

FiberParentClassModelName: FIBERPARENTCLASSMODELNAME

FieldNotesLength: FIELDNOTESLENGTH

GlassLength: GLASSLENGTH

GlobalID: GLOBALID

InstalledBy: FIBERTWOPOINTTRACEFIELD

MultimodeAvailabilityQuantity: FIBERTWOPOINTTRACEFIELD, MULTIMODEAVAILABILITY

OverheadUnderground: OVERHEADUNDERGROUND, FIBERTWOPOINTTRACEFIELD

SegmentGlassLength: SEGMENTGLASSLENGTH

SegmentLength: SEGMENTLENGTH

SinglemodeAvailabilityQuantity: FIBERTWOPOINTTRACEFIELD, SINGLEMODEAVAILABILITY

StartingCableLengthMarking: STARTFOOTSTAMP

ThisFiberClassModelName: THISFIBERCLASSMODELNAME

Object AutoUpdaters

On Feature Create: ArcFM Fiber Optic Cable Length

On Feature Update: ArcFM Fiber Optic Cable Length

On Feature Delete: ArcFM Fiber Object Deleted

After Feature Split: ArcFM Validate Fiber Sheath Split

Field Autoupdaters

ChangeDate — On Feature Update: ArcFM Current Date

ChangeUser — On Feature Update: ArcFM Login User Name

CreationDate — On Feature Create: ArcFM Current Date

CreationUser — On Feature Create: ArcFM Login User Name

DocumentHotLinkPath — Custom Field Editor: ArcFM File Picker

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.