F_Rack_PatchPanel

You can find existing relationships and create new ones in ArcCatalog. Almost all relationships are found at the geodatabase level, as opposed to the dataset level. Below is an image of the final properties for this relationship. For more information about these settings, see the relationship topic Summary of Recommendations.

Because this is a parent/child relationship, it requires the following autoupdater set at the relationship itself:

  • On Relationship Created: ArcFM Update Fiber Parent Field

  • On Relationship Deleted: <None>

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.