Fiber Patch Panel Card Model

TIP: This domain is not required, but you can use it to catalog the model names or numbers for patch panel cards.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

PP Card Model #1

PP Card Model #1

PP Card Model #1

PP Card Model #1

PP Card Model #1

PP Card Model #1

PP Card Model #1

PP Card Model #1

Other

Other

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.