Fiber Patch Panel Card Manufacturer

TIP: This domain is not required, but you can use it to track manufacturers, which would make future queries easier.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

ADC

ADC

AFL

AFL

AMP

AMP

Corning

Corning

Fiberdyne

Fiberdyne

FIS

FIS

Leviton

Leviton

Panduit

Panduit

PLP

PLP

Siecor

Siecor

Tyco

Tyco

Other

Other

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.