Fiber Device Model

TIP: This domain is not required but can help you track fiber optic devices in your network. For example, in the example Coded Values, RS900 is an ethernet switch, and SG2000 is a node station.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

RS900

RS900

RSG2100

RSG2100

RSG2200

RSG2200

RX1000

RX1000

SG2000

SG2000

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.