Fiber Sides

TIP: This domain is not required, but it is helpful to ensure data accuracy when building patch locations and seeing their layout in Patch Panel Connection Reports. Read Fiber Sides and Patch Panel Connection Reports for more information.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

F

Front

B

Back

FB

Front and Back

L

Left

R

Right

LR

Left and Right

FBLR

Front Back Left and Right

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.