Yes / No

TIP: This domain is not required though Fiber Manager works more effectively when this domains is assigned to fields such as DemarcationIndicator in the F_FRONTSIDEPORT table.

Properties:

  • Field Type: Integer

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

0

No

1

Yes

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.