Fiber Fault Status

TIP: This field is not required but helps track the status of faulty or damaged fiber.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Confirmed

Confirmed

Probable

Probable

Repair Complete

Repair Complete

Suspected

Suspected

Ticket Closed

Ticket Closed

Under Repair

Under Repair

Other

Other

Unknown

Unknown

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.