Fiber Device Parent

TIP: This domain is not required but can be used to assign to devices for indicating, when applicable, that the parent is a rack or a patch location.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

RACK

Rack

FIBERPATCHLOCATION

Fiber Patch Location

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.