Create and Configure Tables

This topic contains object classes that are used by the classic fiber data model. You can also find these tables in the Minerville.mdb sample geodatabase. You can choose to create each of these tables manually in ArcCatalog, or use Option 1 to import the schema from Minerville.

Refer to the Basic Fiber Manager Configuration page to configure fields on new object classes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.