Live Swap: Add, Remove, or Replace a Power Module
DISCLAIMER:
-
Electrical equipment should be installed, operated, serviced, maintained, replaced, or have similar work carried out on it only by suitably qualified, trained, experienced, and competent personnel who hold any necessary authorizations (e.g. licenses, permits or certifications) to perform such work. All work must be carried out in a way that does not give rise to danger and using appropriate personal protective equipment (PPE).
-
User must ensure compliance with the manufacturer’s instructions and user manual and with all applicable laws, regulations, standards, and guidance when using this equipment and carrying out work or permitting work to be carried out on or near electrical equipment.
-
Neither Schneider Electric nor any of its affiliates shall be liable for any claims, costs, losses, damages, death, or injuries arising out of the improper use of this equipment or any failure to comply with any of the above requirements.
DANGER |
---|
Hazard of electric shock, explosion, or arc flash
Failure to follow these instructions will result in death or serious injury.
|
WARNING |
---|
risk of equipment damage
Failure to follow these instructions can result in death, serious injury, or equipment
damage.
|
CAUTION |
---|
Heavy load
Power modules are heavy and require two persons to lift.
Failure to follow these instructions can result in injury or equipment damage.
|
-
Check and verify that the remaining power modules can support the load before removing a power module from the UPS.
-
Increasing or decreasing the number of installed power modules in the UPS can only be performed on the scalable UPS models (GVSUPS50K150HS, GVSUPS50K150GS, or GVSUPS25K75FS). Check and verify that the installation is correctly sized for the increase in power rating before installing more power modules in the UPS. Incorrect sizing of the installation can result in an installation overload. See the installation manual for requirements for upstream and downstream protection, cable sizes, etc.
-
On all non-scalable UPS models, only replacement of already present power modules can be performed.
- Remove a power module:
- Remove the screws and push the unlock switch.
- Pull the power module halfway out. A locking mechanism prevents the power module from being pulled all the way out.
- Release the lock by pressing the release button on both sides of the power module and remove the power module.
- Only on scalable UPS models: If no replacement power module will be installed: Install a filler plate in front of the empty power module slot.
- Install a power module:
- Only on scalable UPS models: To install an additional power module , remove the filler plate from the empty power module slot. Save the filler plate for future use.
- Push the power module into the slot. The enable mechanism will latch when the power module is correctly inserted.
- Install the provided screws in the sides of the power module.
The power module will perform a self-test, automatically reconfigure according to the system, and then go online.
DANGER |
---|
Hazard of electric shock, explosion, or arc flash
All power module slots must have either a power module or a filler plate installed.
Failure to follow these instructions will result in death or serious injury.
|