990-6264H-018

Guidance for Organizing Battery Cables

注記: For third party batteries, use only high rate batteries for UPS applications.
注記: When the battery bank is placed remotely, the organizing of the cables is important to reduce voltage drop and inductance. The distance between the battery bank and the UPS must not exceed 200 m (656 feet). Contact Schneider Electric for installations with a longer distance.
注記: To minimize the risk of electromagnetic radiation, it is highly recommended to follow the below guidance and to use grounded metallic tray supports.
Cable length
<30 m (<98 feet) Not recommended Acceptable Recommended Recommended
31-75 m (99-246 feet) Not recommended Not recommended Acceptable Recommended
76-150 m (247-492 feet) Not recommended Not recommended Acceptable Recommended
151-200 m (493-656 feet) Not recommended Not recommended Not recommended Recommended
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

この情報は役に立ちましたか?