990-55222D-001

Configure the UPS Input

OPMERKING: This configuration is mandatory for correct UPS operation.
  1. Tap Configuration > UPS.
    1. Set the Mains configuration to Single mains or Dual mains.
    2. Select Autostart of the inverter if you want to enable this function. When Autostart of the inverter has been enabled, the inverter will start up automatically when input voltage returns, after a shutdown due to drained battery.
      OPMERKING: Autostart of the inverter is not allowed in a parallel system.
      GEVAAR
      Hazard of electric shock, explosion, or arc flash
      Always perform correct Lockout/Tagout before working on the UPS. A UPS with autostart enabled will automatically restart when the mains supply returns.
      Het niet naleven van deze instructies zal leiden tot de dood of ernstig letsel.
    3. Set Transformer present to No transformer present, Input transformer, Output transformer, or Input and output transformers.
    4. Set Power module redundancy to N+0 or N+1*.
    5. Tap OK to save your settings and then tap the arrow symbol to go to the next page.
  2. On the next page, you can view the following settings:
    1. View if Enable customized input current limitis disabled or enabled. When Enable customized input current limit has been enabled, the input current will be limited to the set maximum values given while the UPS is in inverter operation. This feature can only be enabled and configured by Schneider Electric service.
    2. View the setting for Maximum input current limit in inverter operation (A).
    3. View the setting for Maximum input current limit in inverter operation while on generator (A).
    4. Tap OK to save your settings.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.