0000509775_01_en

Battery Regulations

For battery installation always follow local and national regulations that apply in your local area. For example:

  • ZVEI publication "Instructions for the Safe Handling of Electrolyte for Lead-acid Accumulators."

  • ZVEI publication "Safety Data Sheet on Accumulator Acid (Diluted Sulfuric Acid)."

  • VDE 0510 Part 2: 2001-12, in accordance with EN 50272-2:2001: "Safety Requirements for Secondary Batteries and Battery Installations - Part 2: Stationary Batteries".

  • IEEE Standard 450-2002: "Recommended Practice for Maintenance, Testing and Replacement of Vented Lead Acid Batteries for Stationary Application."

  • IEEE Standard 1188-2005: “Recommended Practice for Maintenance, Testing and Replacement of Valve Regulated Lead Acid Batteries for Stationary Application."

  • IEEE Standard 1375-1998: "Guide for Protection of Stationary Battery Systems

For further information refer to the original equipment manufacturer (OEM) of the batteries for instructions on installation, maintenance, and operation of the batteries.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?