Install Battery Measuring Cables
CAUTION |
|---|
|
INACCURATE MEASUREMENTS
Make sure to tighten the pole screws with the correct torque value for your battery.
Failure to follow these instructions can result in injury or equipment damage.
|
| NOTICE |
|---|
|
Always connect the measuring cable to the right pole, the red cable to the positive
pole and the black cable to the negative pole. If the cable connection is reversed
the integrated fuse can be damaged.
Failure to follow these instructions can result in equipment damage.
|
Follow the procedure to connect the measuring cable for your battery type using the right cable:
-
Attach BC4Bxx Measuring Cable for 1.2–2 V Batteries with 2 Poles
-
Attach BC4Bxx Measuring Cable for 1.2–2 V Batteries with 4 or More Poles
CAUTION