SNMP OID List
There are several object identifiers (OID) available from the G.BMS webmanager via SNMP. The webmanager SNMP access needs to be configured. To view and change the SNMP settings from the web interface navigate to Services > SNMP Agent.
The MIB file can be downloaded from: https://www.se.com/ww/en/product-range-presentation/51172807-gutor-battery-management-system/?parent-subcategory-id=88016.
Settings OIDs
OID Address: 1.3.6.1.2.1.33.5.1 / OID Name: bacsSettings
| OID Address | OID Name |
Description
(read only / read-write) |
Scale [Unit] | Example of Read Value* |
|---|---|---|---|---|
| 1.3.6.1.2.1.33.5.1.1 | bacsModuleType |
Module Type. 0 = C20, 1 = C21, 10 = C30, 20 = C40, 20 = C41.
(read only) |
1 | c20(0) -> Module type C20 |
| 1.3.6.1.2.1.33.5.1.2 | bacsNumStrings |
Number of battery strings.
(read only) |
1 | 2 |
| 1.3.6.1.2.1.33.5.1.3 | bacsNumBatteries |
Total number of batteries.
(read only) |
1 | 18 |
| 1.3.6.1.2.1.33.5.1.4 | bacsBattCap |
Capacity of installed batteries.
(read only) |
1 [Ah] | 50 |
| 1.3.6.1.2.1.33.5.1.5 | bacsLogRate1 |
The configured period between log recordings during normal operation. Period between
log recordings.
(read only) |
1 [s] | 1200 -> 1200 seconds (20 minutes)* |
| 1.3.6.1.2.1.33.5.1.6 | bacsLogRate2 |
The configured period between log recordings during charge or discharge.
(read only) |
1 [s] | (The readings are done as soon as possible.)* |
| 1.3.6.1.2.1.33.5.1.7 | bacsImpcPollRate |
The configured period between internal impedance polls.
(read-write) |
1 [min] | 720 -> 720 minutes (12 hours)* |
| 1.3.6.1.2.1.33.5.1.8 | bacsImpcLowAlarm |
Impedance low alarm level.
(read-write) |
0.01 [mΩ] | 110 -> 1.1 mΩ |
| 1.3.6.1.2.1.33.5.1.9 | bacsImpcHighAlarm |
Impedance high alarm level.
(read-write) |
1 | 5000 -> 50 mΩ |
| 1.3.6.1.2.1.33.5.1.10 | bacsTemperatureLowAlarm |
Temperature alarm below this level.
(read-write) |
0.1 [C° or F°]* | 50 -> 5 C° |
| 1.3.6.1.2.1.33.5.1.11 | bacsTemperatureHighAlarm |
Temperature alarm above this level.
(read-write) |
0.1 [C° or F°]* | 350 -> 35C° |
| 1.3.6.1.2.1.33.5.1.12 | bacsVoltageLowAlarm |
Voltage alarm below this level.
(read-write) |
0.01 [V] | 1200 -> 12 V |
| 1.3.6.1.2.1.33.5.1.13 | bacsVoltageHighAlarm |
Voltage alarm above this level.
(read-write) |
0.01 [V] | 1550 -> 15.5 V |
| 1.3.6.1.2.1.33.5.1.14 | bacsImpcLowWarn |
Impedance low warning level.
(read-write) |
0.01 [mΩ] | 120 -> 1.2 mΩ |
| 1.3.6.1.2.1.33.5.1.15 | bacsImpcHighWarn |
Impedance high warning level.
(read-write) |
0.01 [mΩ] | 4000 -> 40 mΩ |
| 1.3.6.1.2.1.33.5.1.16 | bacsTemperatureLowWarn |
Temperature warning below this level.
(read-write) |
0.1 [C° or F°]* | 100 -> 10 C° |
| 1.3.6.1.2.1.33.5.1.17 | bacsTemperatureHighWarn |
Temperature warning above this level.
(read-write) |
0.1 [C° or F°]* | 300 -> 30 C° |
| 1.3.6.1.2.1.33.5.1.18 | bacsVoltageLowWarn |
Voltage warning below this level.
(read-write) |
0.01 [V] | 1200 -> 12 V |
| 1.3.6.1.2.1.33.5.1.19 | bacsVoltageHighWarn |
Voltage warning above this level.
(read-write) |
0.01 [V] | 1410 -> 14.1 V |
| 1.3.6.1.2.1.33.5.1.20 | bacsTemperatureUnit |
Temperature unit currently in use. 0 = Celsius, 1 = Fahrenheit.
(read-write) |
1 | Celsius(0) |
| 1.3.6.1.2.1.33.5.1.21 | bacsStringVoltageLowAlarm |
The configured alarm threshold for the battery string voltage low alarm.
(read-write) |
0.01 [V] | 10500 -> 105 V |
| 1.3.6.1.2.1.33.5.1.22 | bacsStringVoltageHighAlarm |
The configured alarm threshold for the battery string voltage high alarm.
(read-write) |
0.01 [V] | 13500 -> 135 V |
| 1.3.6.1.2.1.33.5.1.23 | bacsStringVoltageLowWarn |
The configured alarm threshold for the battery string voltage low warning.
(read-write) |
0.01 [V] | 11000 -> 110 V |
| 1.3.6.1.2.1.33.5.1.24 | bacsStringVoltageHighWarn |
The configured alarm threshold for the battery string voltage high warning.
(read-write) |
0.01 [V] | 12500 -> 125 V |
| 1.3.6.1.2.1.33.5.1.25 | bacsStringCurrentDeviationDischargeAlarm |
The configured alarm threshold for the current difference between the battery strings
alarm.
(read-write) |
0.01 [A] | 1000 -> 10 A |
| 1.3.6.1.2.1.33.5.1.26 | bacsStringCurrentDeviationChargeAlarm |
The configured alarm threshold for the charge current difference between the battery
strings alarm.
(read-write) |
0.01 [A] | 1000 -> 10 A |
| 1.3.6.1.2.1.33.5.1.27 | bacsStringCurrentDeviationDischargeWarn |
The configured warning threshold for the charge current difference between the battery
strings warning.
(read-write) |
0.01 [A] | 500 -> 5 A |
| 1.3.6.1.2.1.33.5.1.28 | bacsStringCurrentDeviationChargeWarn |
The configured warning threshold for the charge current difference between the battery
warning.
(read-write) |
0.01 [A] | 500 -> 5 A |
Objects OIDs
OID Address: 1.3.6.1.2.1.33.5.2 / OID Name: bacsObjects
| OID Address | OID Name | Description | Scale [Unit] | Example of Read Value |
|---|---|---|---|---|
| 1.3.6.1.2.1.33.5.2.1 | bacsStatus | G.BMS system status flags. For information about the flags see General Status Flags Description. | (Decimal format) | 65 -> 0x0041 |
| 1.3.6.1.2.1.33.5.2.2 | bacsAvModuleVolt | Average module voltage. | 0.01 [V] | 1287 -> 12.87 V |
| 1.3.6.1.2.1.33.5.2.3 | bacsTotalVolt | Total voltage of all modules. | 0.01 [V] | 23176 -> 231.76 V |
| 1.3.6.1.2.1.33.5.2.4 | bacsNumModules | The number of installed battery modules. | 1 | 18 |
| 1.3.6.1.2.1.33.5.2.5 | bacsModuleTable | The list of battery table entries. | N/A | N/A |
| 1.3.6.1.2.1.33.5.2.5.1 | bacsModuleEntry | An entry containing information applicable to a particular battery. | N/A | N/A |
| 1.3.6.1.2.1.33.5.2.5.1.1 | bacsModuleIndex | The module identifier. | 1 |
|
| 1.3.6.1.2.1.33.5.2.5.1.2 | bacsModuleVoltage | Ordered list of the measured battery voltage by each module. | 0.01 [V] |
|
| 1.3.6.1.2.1.33.5.2.5.1.3 | bacsModuleTemperature | Ordered list of the temperature measured by each module. | 0.1 [C° or F°]* |
|
| 1.3.6.1.2.1.33.5.2.5.1.4 | bacsModuleBypass | Ordered list of the module bypass measured by each module. | 0.1 [%] |
|
| 1.3.6.1.2.1.33.5.2.5.1.5 | bacsModuleResistance | Ordered list of the measured module impedance in each module. | 0.01 [mΩ] |
|
| 1.3.6.1.2.1.33.5.2.5.1.6 | bacsModuleState | The general module alarm flags. For information about the flags see Alarm Flags Description. | (Decimal format) |
|
| 1.3.6.1.2.1.33.5.2.6 | bacsNumStrings | The number of installed battery strings. | 1 | 2 |
| 1.3.6.1.2.1.33.5.2.7 | bacsStringTable | The list of stringy table entries. | N/A | N/A |
| 1.3.6.1.2.1.33.5.2.7.1 | bacsStringEntry | An entry that contains information about a specific string of batteries. | N/A | N/A |
| 1.3.6.1.2.1.33.5.2.7.1.1 | bacsStringIndex | The string identifier. | 1 |
|
| 1.3.6.1.2.1.33.5.2.7.1.2 | bacsStringCurrent | The string current. | 0.01 [A] |
|
| 1.3.6.1.2.1.33.5.2.7.1.3 | bacsStringTotalVolt | The string total voltage. | 0.01 [V] |
|
| 1.3.6.1.2.1.33.5.2.7.1.4 | bacsStringAverageVol | The string average voltage per battery. | 0.01 [V] |
|
| 1.3.6.1.2.1.33.5.2.7.1.5 | bacsStringCurrentAC | The string AC current. | 0.01 [A] |
|
| 1.3.6.1.2.1.33.5.2.7.1.6 | bacsStringAlarm | The general string alarm flags. For information about the flags see Alarm Flags Description. | (Decimal format) |
|
| 1.3.6.1.2.1.33.5.2.7.1.7 | bacsStringAlarm2 | The string alarm flags. For information about the flags see Battery String Alarm Flags Description. | (Decimal format) |
|
Alarm OIDs
OID Address: 1.3.6.1.2.1.33.5.3 / OID Name: bacsAlarms
| OID Address | OID Name | Description |
|---|---|---|
| 1.3.6.1.2.1.33.5.3.1 | bacsAlarmsPresent | The present number of active alarm conditions. |
| 1.3.6.1.2.1.33.5.3.2 | bacsAlarmTable | A list of alarm entries. |
| 1.3.6.1.2.1.33.5.3.2.1 | bacsAlarmEntry | An entry containing information applicable to a particular alarm. |
| 1.3.6.1.2.1.33.5.3.2.1.1 | bacsAlarmId | A unique identifier for an alarm condition. This value must remain constant. |
| 1.3.6.1.2.1.33.5.3.2.1.2 | bacsAlarmDescr | A reference to an alarm description object. The object referenced should not be accessible, but rather be used to provide a unique description of the alarm condition. |
| 1.3.6.1.2.1.33.5.3.2.1.3 | bacsAlarmTime | The value of sysUpTime when the alarm condition was detected. If the alarm condition was detected during the webmanager startup and presumably existed before the webmanager startup, then dcAlarmTime = 0. |
| 1.3.6.1.2.1.33.5.3.3 | bacsWellKnownAlarms | A list of traps, see Alarm Trap List. |
| 1.3.6.1.2.1.33.5.3.4 | bacsModuleAlarmsPresent | The number of G.BMS modules currently in an alarm state. |
| 1.3.6.1.2.1.33.5.3.5 | bacsModuleWarningsPresent | The number of G.BMS modules currently in a warning state. |
Alarm Trap List
OID Address (SNMP Traps): 1.3.6.1.2.1.33.5.3.3 / OID Name: bacsWellKnownAlarms
| OID Address | OID Name | Description |
|---|---|---|
| 1.3.6.1.2.1.33.5.3.3.1 | bacsAlarmSystemError | This object indicates a communication problem from the webmanager to one or more of the battery modules. |
| 1.3.6.1.2.1.33.5.3.3.2 | bacsAlarmResistWarn | This object indicates that the internal resistance of one or more batteries is above the warning level. |
| 1.3.6.1.2.1.33.5.3.3.3 | bacsAlarmResistAlarm | This object indicates that the internal resistance of one or more batteries is above the alarm level. |
| 1.3.6.1.2.1.33.5.3.3.4 | bacsAlarmVoltage | This object indicates that the voltage of one or more batteries is outside the defined rage. |
| 1.3.6.1.2.1.33.5.3.3.5 | bacsAlarmTemperature | This object indicates that the temperature of one or more batteries is outside the defined range. |
| 1.3.6.1.2.1.33.5.3.3.6 | bacsAlarmVoltageHigh | This object indicates that the voltage of one or more batteries is higher than the defined range. |
| 1.3.6.1.2.1.33.5.3.3.7 | bacsAlarmVoltageLow | This object indicates that the voltage of one or more batteries is lower than the defined range. |
| 1.3.6.1.2.1.33.5.3.3.8 | bacsAlarmTemperatureHigh | This object indicates that the temperature of one or more batteries is higher than the defined range. |
| 1.3.6.1.2.1.33.5.3.3.9 | bacsAlarmTemperatureLow | This object indicates that the temperature of one or more batteries is lower than the defined range. |
| 1.3.6.1.2.1.33.5.3.3.10 | bacsAlarmResistAlarmHigh | This object indicates that the internal resistance of one or more batteries is above the alarm level. |
| 1.3.6.1.2.1.33.5.3.3.11 | bacsAlarmResistAlarmLow | This object indicates that the internal resistance of one or more batteries is below the alarm level. |
| 1.3.6.1.2.1.33.5.3.3.12 | bacsAlarmEqualizing | This object indicates that the equalizing is not operating correctly. |
| 1.3.6.1.2.1.33.5.3.3.13 | bacsAlarmVoltageWarnHigh | This object indicates that the voltage of one or more batteries is higher than the defined warning range. |
| 1.3.6.1.2.1.33.5.3.3.14 | bacsAlarmVoltageWarnLow | This object indicates that the voltage of one or more batteries is lower than the defined warning range. |
| 1.3.6.1.2.1.33.5.3.3.15 | bacsAlarmTemperatureWarnHigh | This object indicates that the temperature of one or more batteries is higher than the defined warning range. |
| 1.3.6.1.2.1.33.5.3.3.16 | bacsAlarmTemperatureWarnLow | This object indicates that the temperature of one or more batteries is lower than the defined warning range. |
| 1.3.6.1.2.1.33.5.3.3.17 | bacsAlarmResistWarnHigh | This object indicates that the internal resistance of one or more batteries is higher than the defined warning range. |
| 1.3.6.1.2.1.33.5.3.3.18 | bacsAlarmResistWarnLow | This object indicates that the internal resistance of one or more batteries is lower than the defined warning range. |
| 1.3.6.1.2.1.33.5.3.3.19 | bacsAlarmInitializing | The webmanager is initializing. |
| 1.3.6.1.2.1.33.5.3.3.20 | bacsAlarmCommunicationLost | BACS bus communication is lost. |
| 1.3.6.1.2.1.33.5.3.3.21 | bacsAlarmBatteryBreakerOpen | Battery breaker is open. |
| 1.3.6.1.2.1.33.5.3.3.22 | bacsAlarmThermalRunaway | Thermal runaway detected. |
| 1.3.6.1.2.1.33.5.3.3.23 | bacsAlarmSensorCommunicationLost | Sensor communication is lost. |
| 1.3.6.1.2.1.33.5.3.3.24 | bacsAlarmDischarging | Batteries are being discharged. |
| 1.3.6.1.2.1.33.5.3.3.25 | bacsAlarmDischargingStopped | Batteries are no longer being discharged. |
| 1.3.6.1.2.1.33.5.3.3.26 | bacsAlarmMaxVoltageDiff | The voltage difference is too high. |
| 1.3.6.1.2.1.33.5.3.3.27 | bacsAlarmStringVoltHigh | The battery string voltage is above the configured alarm threshold. |
| 1.3.6.1.2.1.33.5.3.3.28 | bacsAlarmStringVoltLow | The battery string voltage is below the configured alarm threshold. |
| 1.3.6.1.2.1.33.5.3.3.29 | bacsAlarmStringVoltHighWarn | The battery string voltage is above the configured warning threshold. |
| 1.3.6.1.2.1.33.5.3.3.30 | bacsAlarmStringVoltLowWarn | The battery string voltage is below the configured warning threshold. |
| 1.3.6.1.2.1.33.5.3.3.31 | bacsAlarmStringCurrentHigh | The battery string current is above the configured alarm threshold. |
| 1.3.6.1.2.1.33.5.3.3.32 | bacsAlarmStringCurrentLow | The battery string current is below the configured alarm threshold. |
| 1.3.6.1.2.1.33.5.3.3.33 | bacsAlarmStringCurrentHighWarn | The battery string current is above the configured warning threshold. |
| 1.3.6.1.2.1.33.5.3.3.34 | bacsAlarmStringCurrentLowWarn | The battery string current is below the configured warning threshold. |
| 1.3.6.1.2.1.33.5.3.3.35 | bacsAlarmStringEqualizingDisabled | The battery string equalizing is disabled. |
| 1.3.6.1.2.1.33.5.3.3.36 | bacsAlarmStringCurrDeviationCharge | The charge current difference between the battery strings is above the configured alarm threshold. |
| 1.3.6.1.2.1.33.5.3.3.37 | bacsAlarmStringCurrDeviationDischarge | The discharge current difference between the battery strings is above the configured alarm threshold. |
| 1.3.6.1.2.1.33.5.3.3.38 | bacsAlarmStringCurrDeviationChargeWarn | The charge current difference between the battery strings is above the configured warning threshold. |
| 1.3.6.1.2.1.33.5.3.3.39 | bacsAlarmStringCurrDeviationDischargeWarn | The discharge current difference between the battery strings is above the configured warning threshold. |
Traps OIDs
OID Address (SNMP Traps): 1.3.6.1.2.1.33.5.4 / OID Name: bacsTraps
| OID Address | OID Name | Description |
|---|---|---|
| 1.3.6.1.2.1.33.5.4.1 | bacsTrapAlarmEntryAdded | Sent when an alarm in the system appears. |
| 1.3.6.1.2.1.33.5.4.2 | bacsTrapAlarmEntryRemoved | Sent when an alarm in the system disappears. |
GX_R_AUX OIDs
OID Address: 1.3.6.1.2.1.33.5.5 / OID Name: gxRAUX
| OID Address | OID Name | Description | Example of Read Value |
|---|---|---|---|
| 1.3.6.1.2.1.33.5.5.1 | gxRAUX1Input1 | Status of input 1 on GX_R_AUX 1. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.2 | gxRAUX1Input2 | Status of input 2 on GX_R_AUX 1. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.3 | gxRAUX1Input3 | Status of input 3 on GX_R_AUX 1. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.4 | gxRAUX1Input4 | Status of input 4 on GX_R_AUX 1. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.5 | gxRAUX1Output1 | Status of output 1 on GX_R_AUX 1. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.6 | gxRAUX1Output2 | Status of output 2 on GX_R_AUX 1. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.7 | gxRAUX1Output3 | Status of output 3 on GX_R_AUX 1. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.8 | gxRAUX1Output4 | Status of output 4 on GX_R_AUX 1. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.9 | gxRAUX2Input1 | Status of input 1 on GX_R_AUX 2. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.10 | gxRAUX2Input2 | Status of input 2 on GX_R_AUX 2. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.11 | gxRAUX2Input3 | Status of input 3 on GX_R_AUX 2. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.12 | gxRAUX2Input4 | Status of input 4 on GX_R_AUX 2. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.13 | gxRAUX2Output1 | Status of output 1 on GX_R_AUX 2. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.14 | gxRAUX2Output2 | Status of output 2 on GX_R_AUX 2. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.15 | gxRAUX2Output3 | Status of output 3 on GX_R_AUX 2. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.16 | gxRAUX2Output4 | Status of output 4 on GX_R_AUX 2. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.17 | gxRAUX3Input1 | Status of input 1 on GX_R_AUX 3. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.18 | gxRAUX3Input2 | Status of input 2 on GX_R_AUX 3. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.19 | gxRAUX3Input3 | Status of input 3 on GX_R_AUX 3. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.20 | gxRAUX3Input4 | Status of input 4 on GX_R_AUX 3. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.21 | gxRAUX3Output1 | Status of output 1 on GX_R_AUX 3. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.22 | gxRAUX3Output2 | Status of output 2 on GX_R_AUX 3. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.23 | gxRAUX3Output3 | Status of output 3 on GX_R_AUX 3. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.24 | gxRAUX3Output4 | Status of output 4 on GX_R_AUX 3. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.25 | gxRAUX4Input1 | Status of input 1 on GX_R_AUX 4. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.26 | gxRAUX4Input2 | Status of input 2 on GX_R_AUX 4. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.27 | gxRAUX4Input3 | Status of input 3 on GX_R_AUX 4. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.28 | gxRAUX4Input4 | Status of input 4 on GX_R_AUX 4. | normal ( 1 ) |
| 1.3.6.1.2.1.33.5.5.29 | gxRAUX4Output1 | Status of output 1 on GX_R_AUX 4. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.30 | gxRAUX4Output2 | Status of output 2 on GX_R_AUX 4. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.31 | gxRAUX4Output3 | Status of output 3 on GX_R_AUX 4. | off ( 0 ) |
| 1.3.6.1.2.1.33.5.5.32 | gxRAUX4Output4 | Status of output 4 on GX_R_AUX 4. | off ( 0 ) |