0000509775_01_en

Splitting Box Technical Data and Parts

Dimension (L x W x H) 92 x 67 x 25 mm (3.6 x 2.6 x 0.98 in)
Protection rating IP 40
Fastening With an additional mounting clip it can be attached to a DIN rail, see Mounting Clip.
Certifications UL, CSA and CE

Splitting Box Parts

Part Number Part Name Description
950-6506 BMS BACS PASSIVE SPLITTING BOX Passive device, does not need any power supply.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?