0000509775_01_en

Check Battery Setup Settings

To check the battery setup settings:

  1. Navigate to Devices > BACS > Setup from the side menu.

  2. Here it is possible to view the battery/module setup.

  3. Make sure that the settings are correct, or if necessary make any changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?