0000509775_01_en

Configure and Change Settings from the Web Interface

The initial startup defined some basic settings in the System Setup Wizard. It is possible to change these settings and to change additional settings from the web interface.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?