0000509775_01_en

Install Stand-Alone Temperature and Humidity Sensor

A stand-alone temperature and humidity sensor needs to be connected directly to the COM2 port on the webmanager with the included mini-DIN-8/DB-9 cable. The maximum cable length for connections to COM2 is 15 m (49 ft).

NOTE: There is only one COM2 port so it is only possible to connect one stand-alone temperature and humidity sensor to a webmanager.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?