Initial Local Connection to the Webmanager
First login with default IP address:
-
Check that the webmanager slide switch is in the left position.
-
Connect your workstation to the webmanagers LAN port with an Ethernet cable, directly or through a switch.
-
On your workstation run Command Prompt as administrator.
-
In the Command Prompt window type
route add 10.10.10.10 xxx.xxx.xxx.xxx, wherexxx.xxx.xxx.xxxis the local IP of your workstation. -
Press Enter. A success confirmation will be shown in the Command Prompt window.
-
Open a web browser from your workstation.
-
Enter
https://10.10.10.10in the browser address field. A login window will open. -
In the login window enter:
- User: admin
- Password: cs141-snmp
NOTE: After the first log in the user is prompted and required to set a new password. -
The first login will run the System Setup Wizard that will help you setup the basic configurations of the webmanager.
NOTE: If the System Setup Wizard does not start automatically on the first login you can launch it by clicking System > Wizard