0000509775_01_en

EcoStruxure and Digital Integration

The webmanagers Modbus or SNMP settings can be configured for integration with EcoStruxure Grid (Modbus), EcoStruxure Power (Modbus), EcoStruxure IT (SNMP), AVEVA or other third-party solutions. For the setup refer to the documentation for the respective solution.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?