0000509775_01_en

Prepare the Batteries

Before you attach the G.BMS module fastening strips the battery surface must be clean and dry. To clean the battery surface:

  1. Check what cleaning product is recommended by the battery manufacturer.

    NOTE: If you are unsure or there are no recommendations available use only soapy water.

  2. Clean the surface of the batteries with the recommended cleaning product.

  3. Dry the surface of the batteries with an antistatic fabric.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?