0000509775_01_en

General Placement Information

The recommended placement is on top of the battery.

If there is not enough space on the top of the battery, place the G.BMS module on the front panel of the battery.

NOTE: It is recommended to place the modules with the measuring cables in a loop with the connection pointing down. This reduces the risk of any gas condensate dripping into the connection.

Do not place the G.BMS modules on any cooling ribs or plugs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?