0000509775_01_en

Attach BC5xx Measuring Cable for 4–16 V Batteries

  • (A) Pole screw
  • (B) Safety washer
  • (C) Washer
  • (D) Measuring cable
  • (E) Battery connector
  • (F) Battery pole
IMPORTANT: Attach the cable as close as possible to the battery poles, but above the battery connectors.

To attach the BC5xx measuring cable to the battery:

  1. Connect the red cable to the positive battery pole.
  2. Connect the black cable to the negative battery pole.
  3. Tighten the pole bolts with the torque value recommended by the battery manufacturer.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?