0000509775_01_en

Program a Single Module

IMPORTANT: Make sure only a single module is connected to the webmanager.
NOTE: The programmer mode in the programmer page must be toggled On to find the address of a single module or to program a single module.

Check the Currently Programed Address of a Single Module

From the programmer page:

  1. Under the Address section click Search

  2. A progress bar will appear and after a short while the address of the single connected module will be shown.

Change the Currently Programed Address of a Single Module

From the programmer page:

  1. Under the Single section, in the Old field enter the current module address.

  2. In the New field enter the new target address for the module.

  3. Click Set to confirm the new address for the module.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?