0000509775_01_en

Install Additional Options

Depending on the sensor or device different fastening options exists, for example DIN rail 35 x 7.5 mm (TS35 rail), wall mounted or adhesive. For more information see the respective section in Technical Data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?