Add Sensors and Devices
Any sensor or other device used in the G.BMS needs to be added before it can be configured from the web interface.
To add a sensor or device:
-
Check that the sensor or device is correctly connected to the webmanager, either to COM2 or via the BACS bus to a battery bus (COM3) port. This depends on the type of sensor or device and the cable needed.
-
If multiple current sensors or GX_R_AUX devices are connected to the same webmanager check that they have unique addresses configured with the DIP switches.
-
Navigate to Devices > Setup.
- Under COM2 or COM3 use the drop-down menu(s) to select the connected sensor or device.
-
Click Apply to add the sensor or device.
-
A new setup menu or submenu under Devices is added for that sensor or device. From this new menu the sensor or device can be configured as needed.