EIO0000003565_05

Replacing the System Card (SD Card)

The System Card is an SD Card with the operating system installed on it.

To replace the System Card, use a SD Card by Schneider Electric. Refer to Accessories.

NOTICE
LOSS OF DATA
When using a SD Card:
  • Make sure you regularly back up the SD Card data.
  • While a SD Card is accessed, do not turn OFF or reset this product, and do not remove the SD Card.
  • Before removing the SD Card from this product, stop all operations on the SD Card.
  • Make sure of the SD Card’s orientation before inserting it into the SD Card slot.
Failure to follow these instructions can result in equipment damage.
NOTE: For information on backing up your SD card, used as a system card, refer to our website at www.se.com.
NOTICE
LOSS OF DATA
When handling the SD Card:
  • Avoid storing the SD Card where there is static electricity or electromagnetic waves.
  • Avoid storing the SD Card in direct sunlight, near a heater, or other locations where high temperatures can occur.
  • Do not bend the SD Card.
  • Do not drop or strike the SD Card against another object.
  • Keep the SD Card dry.
  • Do not touch the SD Card connectors.
  • Do not disassemble or modify the SD Card.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

Turn OFF this product.

2

Remove the Box Module from the Display Module.

NOTE: Refer to Installation.

3

As illustrated, open the System Card Cover in the direction of the arrow.

1 System Card Cover

2 Box Module

4

Push the SD Card once to release, and pull out the card.

NOTE: After using the SD Card, store the SD Card in its case or other safe location.

5

Insert the SD Card into the System Card Slot with the front face of the SD Card facing down, and push until you hear it “click”.

1 System Card Slot

6

Close the System Card Cover.

7

Mount the Box Module on the Display Module.

NOTE: As shown in the image below (example on the left-hand side), you can set the Write-Control Tab to prevent write operations to the SD Card. Push the tab up, as shown in the example on the right-hand side, to release the lock and enable writing to the SD Card.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.