EIO0000003565_05

Removing the SD Card

If you remove the SD Card while it is in use, you risk corrupting your data. Before removing the SD Card from this product, stop all operations on the SD Card.

For instructions on removing the SD Card safely, refer to the corresponding topic in the manual of your screen editing software.

Step

Action

1

Make sure the Card Access LED is off.

1 Card access LED

2

Open the Storage Card Cover.

1 Storage card cover

3

Push the SD Card once to release, and pull out the card.

NOTE: After using the SD Card, store the SD Card in its case or other safe location.

4

Close the Storage Card Cover.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.