EIO0000003565_05

Replacing the Installation Gasket

Introduction

The installation gasket provides protection against dust and moisture.

NOTICE
GASKET AGING
  • Inspect the gasket periodically as required by your operating environment.
  • Replace the gasket at least once a year, or as soon as scratches or dirt become visible.
Failure to follow these instructions can result in equipment damage.

Installing the Installation Gasket

Stage

Description

1

Place the Display Module on a flat, level surface, with the display face pointing down.

2

Remove the gasket from the Display Module.

3

Attach the new gasket to the Display Module. Insert the protrusions from the four corners of the gasket into the corresponding holes in the corners of the Display Module.

Depending on your model, there may be additional protrusions. In the following, refer to the figure on the right and insert the protrusions accordingly.

NOTE: When using a tool to insert the gasket, make sure the tool does not catch the rubber gasket and cause a tear.

1 Installation gasket

2 Protruduing point

The gasket must be inserted correctly into the groove for moisture resistance for the Display Module.

NOTICE
EQUIPMENT DAMAGE
Be careful not to stretch the gasket unnecessarily.
Failure to follow these instructions can result in equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.