Introduction
This product is designed for use on flat surfaces of IP66F, IP67F, Type 4X (indoor and outdoor use), Type 12 and Type 13 enclosures.
Mount this product in an enclosure that provides a clean, dry, robust and controlled environment.
Be aware of the following when building this product into an end-use product:
-
The rear face of eXtreme Display and all faces of eXtreme Box are not approved as an enclosure. When building this product into an end-use product, be sure to use an enclosure that satisfies standards as the end-use product’s overall enclosure.
-
Install this product in an enclosure with mechanical rigidity.
-
The front face of eXtreme Display is designed for indoor and outdoor use, and for use in a wet location. UL certification obtained is for indoor and outdoor use for the front side, and indoor use only for other sides.
-
eXtreme Box is not designed for outdoor use. UL certification obtained is for indoor use only.
-
Install and operate this product with its front panel facing outward.