EIO0000003565_05

Auxiliary Output/Speaker Output Interface (AUX)

DANGER
ELECTRIC SHOCK AND FIRE
When using the SG terminal to connect an external device to this product:
  • Verify that a ground loop is not created when you set up the system.
  • Connect the SG terminal to remote equipment when the external device is not isolated.
  • Connect the SG terminal to a known reliable ground connection to reduce the risk of damaging the circuit.
Failure to follow these instructions will result in death or serious injury.

Cable connection side

Pin No.

Signal name

Direction

Meaning

1

LineOut

Output

Line Out

2

LineOut_GND

Output

Line Out Ground

3

SP+

Output

Speaker +

4

SP-

Output

Speaker -

5

NC

No Connection

6

ALARM+/ BUZZER+

Output

(Can be changed via software)

7

ALARM-/ BUZZER-

Output

AUX Connector: HMIZGAUX by Schneider Electric

Output Circuit

A Internal Circuit

B Pin Number 6: ALARM+/BUZZER+

C Pin Number 7: ALARM-/BUZZER-

D Load

E External Power

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.