EIO0000003565_05

Attaching Fixing Bracket (HMIDT35X )

By using the fixing bracket optional part (part number: HMIZXFIX1), you can secure the Box Module to the Display Module.

Step

Action

1

Hook the end of the fixing bracket in the ventilation hole at the top of the Display Module, and use a screw (1 piece) to secure the fixing bracket to the back of the Box Module. The necessary torque is 0.5 N•m (4.4 lb-in).

1 Fixing bracket

2 Ventilation hole

NOTICE
EQUIPMENT DAMAGE
Do not exert more than 0.5 N•m (4.4 lb-in) of torque when tightening the screw.
Failure to follow these instructions can result in equipment damage.
NOTE: When the fixing bracket is attached, you cannot attach the isolation unit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.