EIO0000003565_05

Removing from the Panel

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
Failure to follow these instructions will result in death or serious injury.
CAUTION
RISK OF INJURY
Do not drop this product when you remove it from the panel.
  • Hold this product in place after removing the fasteners.
  • Use both hands.
  • While pushing on the anti-drop lock, be careful not to hurt your fingers.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
EQUIPMENT DAMAGE
To avoid damage, remove this product while pushing the anti-drop lock or by making sure the lock does not touch the panel.
Failure to follow these instructions can result in equipment damage.
NOTICE
EQUIPMENT DAMAGE
  • When this product is mounted vertically, first remove the Display Module from the panel, then remove the Box Module from the Display Module.
  • Keep this product stabilized in the panel cutout while you are installing or removing the screw fasteners.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

Using a Phillips screwdriver, gradually loosen (turn counterclockwise) the screws for the fasteners (top, bottom, left, and right), alternating diagonally between screws until all screws are loose.

1 Rear side

NOTE:
  • For the number of installation fasteners on your model, see Number of Installation Fasteners in Step 5 of Installing to the Panel.

  • If the panel is thick (approximately 5 mm [0.2 in]), you may have trouble straightening the L-shaped part of the installation fastener. If this happens, push the display module from the front as you loosen the screws.

2

While pushing on the anti-drop lock on the top of the Display Module with a tool such as a screwdriver, slowly remove the Display Module from the panel.

1 Panel

2 Front side

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.