EIO0000003565_05

Inserting the SD Card

NOTE: As shown in the image below (example on the left-hand side), you can set the Write-Control Tab to prevent write operations to the SD Card. Push the tab up, as shown in the example on the right-hand side, to release the lock and enable writing to the SD Card. Before using a commercial-type SD Card, read the manufacturer's instructions.

Step

Action

1

Open the Storage Card Cover.

1 Storage card cover

2

Insert the SD Card into the SD Card Slot with the front face of the SD Card facing up and push until you hear it “click”.

3

Close the Storage Card Cover.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.