EIO0000003565_05

Installing to the Panel

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • Remove all power from the device before removing any covers or elements of the system, and prior to installing or removing any accessories, hardware, or cables.
  • Unplug the power cable from both this product and the power supply prior to installing or removing the product.
  • Always use a properly rated voltage sensing device to confirm power is off where and when indicated.
  • Replace and secure all covers or elements of the system before applying power to this product.
Failure to follow these instructions will result in death or serious injury.
NOTICE
EQUIPMENT DAMAGE
  • When mounting this product vertically, install the Box Module onto the Display Module before attaching the Display Module to the panel.
  • Keep this product stabilized in the panel-cut while you are installing or removing the screw fasteners.
Failure to follow these instructions can result in equipment damage.

Step

Action

1

When mounting this product vertically, place the Display Module on a clean and level surface with the screen facing down and mount the Box Module to the Display Module. Refer to Installing onto Display Module.

2

Check that the Display Module’s gasket is seated securely into the bezel’s groove, which runs around the perimeter of the display panel frame.

NOTE: Always use the installation gasket, since it absorbs vibration in addition to repelling water. For the procedure on replacing the installation gasket, refer to Replacing the Installation Gasket.

3

Based on the Display Module's Panel Cut Dimensions, open a mount-hole on the panel and attach the Display Module to the panel from the front side.

4

Confirm that the anti-drop lock on the top of the Display Module is attached to the panel.

Except for HMIDT35X

HMIDT35X

1 Anti-drop lock

2 Panel

5

Using a Phillips screwdriver, gradually tighten (turn clockwise) the screws for the fasteners (top, bottom, left, and right), alternating diagonally between screws until all are secure. Be sure that the L-shaped part of the installation fastener (2 in figure below) is completely vertical. The necessary torque is 0.7 N•m (6.2 lb-in).

NOTE:
  • If the Display Module is not mounted properly, it may fall.

  • If the panel is thick (approximately 5 mm [0.2 in]), you may have trouble straightening the L-shaped part of the installation fastener. If this happens, push the display module from the front as you tighten the screws.

1 Installation fastener

2 L-shaped part of the installation fastener

Number of Installation Fasteners

15-inch or larger models:

  • Top - 2, Bottom - 2, Right - 2, Left - 2

Models less than 12-inch:

  • Top - 2, Bottom - 2, Right - None, Left - None

NOTICE
EQUIPMENT DAMAGE
Do not exert more than 0.7 N•m (6.2 lb-in) of torque when tightening the fastener's screws.
Failure to follow these instructions can result in equipment damage.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?